Using "HAL_CAN_AddTxMessage" from interrupt and main loop
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-05 5:25 AM
Hi, I want to be able to add CAN message with "HAL_CAN_AddTxMessage" from interrupt and main loop (loop maybe busy sometimes so I cant send all messages from it). I assume they can collide and override so its not safe to do it from both?
What are my options?
Triggering software interrupt and somehow passing data from interrupt/main loop? (not sure how to pass data as it can be overwritten)
Timer interrupt which always checks if data is needed to be sent every 10ms or so?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0