cancel
Showing results for 
Search instead for 
Did you mean: 

Using FATFS with stm32f4, adjust cluster size

hariprasad
Associate III
Posted on June 09, 2015 at 07:05

Hi ,

I am using chan's FATFS with stm32f4 discovery,, So I could see that two paramateres,

&sharpdefine    _MAX_SS        512

and

&sharpdefine BLOCK_SIZE            512

But when I change it to 4096 the FS is no longer able to open a File,

Is the changing of these parameters advisable ?

#stm32f4 #gpio #dma #discovery
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0