cancel
Showing results for 
Search instead for 
Did you mean: 

Using a 32F469I-DISCOVERY board, is there any examples of creating a two output one-pulse timer with an external input? I am having trouble with the Arduino connector on the back of the board to pinout the three signals.

CSche.4
Associate III

Also how to internally connect the input trigger to two simultaneous one-pulse generators. 

2 REPLIES 2

There really isn't an internal connectivity fabric

The TIM can cross their own CH1/CH2 and CH3/CH4 channels (direct/in-direct), and there is some input/output triggering plumbing which connect specific TIM/CH between each other.

The AF MUX fabric really only allows for a single peripheral connection to a pin.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
CSche.4
Associate III

is this the correct set up for a one-pulse?0693W00000GWrmfQAD.jpgdoes not seem to work.