2019-03-11 12:39 AM
Dear Members,
I want to read a result from my GPS,
it's Neo 6M
I initialized 2 UARTs UART 1 for PC and UART 2 for GPS,
I got this result :
INIT CODE GPS NEO - 6M....
From GPS :
Is it receiving properly ?
The code :
char in[8];
printf("From GPS : ");
HAL_UART_Receive(&huart2, (uint8_t *)in, 8, 1000);
HAL_UART_Transmit(&huart1, (uint8_t *)in, 8, 1);
printf("\r\n");
Green LED on GPS module is blinking...
Thanks
2019-03-11 4:15 AM
I would expect NMEA sentences at 9600 8N1
Your HAL functions block, so no ideal for forwarding data.
2019-03-11 4:24 AM
> I would expect NMEA sentences at 9600 8N1
This are the default setting of the module.
Do you have the baudrate of the STM32 MCU set properly ?
And not changed the module's setting to binary UBX messages ?
In addition to the inappropriateness of said HAL functions.
2019-03-11 4:43 AM
Seems too consistent and wrong data to be UBX. Would need to know more about specific implementation. NAZA UAV modules for example output their own packet format.
One could observe data with a scope, or use USB to CMOS Serial directly from NEO-6M module.
2019-03-11 4:47 AM
Does the receive call function or does it return an error? Try clearing the buffer and checking. Post lacks a lot of salient details which would help diagnose situation.
To answer the underlying question, No this doesn't look to be receiving properly/correctly.
2019-03-11 5:11 AM
void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
}
/* USART2 init function */
void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
//huart2.Init.BaudRate = 115200;
huart2.Init.BaudRate = 9600;//NEO6M Baudrate
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
}UART Setting from STM32CubeMX
@Clive
Which UART buffer should I clear ?
2019-03-11 5:16 AM
I'm using the module indoor, does it receive signal ?
Or without a signal, at least I can read its ID with UART ?
Is this the right manual ?
or there's another more comprehensive one ?
Thanks
2019-03-11 5:17 AM
the module is like this :
2019-03-11 5:18 AM
2019-03-14 2:35 AM
I got output from
serial to PC
May be with interrupt is better ?
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
display to pc here
}