cancel
Showing results for 
Search instead for 
Did you mean: 

Use P-NUCLEO-53L1A1 to be fall-detection and put on wall, possible?

leo su
Associate II
Posted on March 15, 2018 at 11:27

Description:

We currently use P-NUCLEO-53L1A1 (3 sesnors) to be a fallen-detection sensor product.

Instead of putting this interior of ceiling (coz sometimes it has height problem for installing),

we plan to put it into wall with 4 sensors (each sensor has 27degree view, so if we put 4 sensors onto wall)

and is it possible to check ranging distance via horizontal view instead of vertical? Any experience sharing.. thx

Motive:

Take 4 ranging sensors onto wall instead of setting up them onto ceiling, any difference or feasibility

problem for this idea?
3 REPLIES 3
Andrew Neil
Evangelist III
Posted on March 15, 2018 at 13:07

Surely, the whole point of an Evaluation tool like the 

P-NUCLEO-53L1A1 is to let you try it out - in other words, to Evaluate whether it works?

The clue is in the name!

leo su
Associate II
Posted on March 15, 2018 at 18:36

Hi Andrew,

Not clear about ur explanation, 

as my checking situation, we use it as a ranging sensor device set-up at top of ceiling so any object is moving around

below device or fall-down or even jumping can be scanned and distance difference found by a vertical view.

However, if we put sensor device at higher wall instead of ceiling, when object or person is trying to moving or falling down,

is a horizontal view of sensors can easily find it same as a set-up at ceiling???
Posted on March 15, 2018 at 20:02

Andrew's point is that you get to evaluate YOUR use case. You're going to need to point the sensors at the things/distances you want to measure for them to be effective.

You'd be better off posting to the right forum, or discussing with the engineers supporting your account.

https://community.st.com/community/mems-sensors-community/mems-sensors-forum

kvam.johne

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..