Skip navigation
Log in to follow, share, and participate in this community.

Recent Activity

EL KHABLI AHMED
Hello I want to detect the movement for 10 min from an accelerometer LIS2DE12, I want to know if I can use the configuration of the interuption register or i must use a REal time counter  Thanks
in MEMS and Sensors Forum
Jumshed Akhtar
Hi I am using  LPS22HB with my custom made board based on STM32F777. I am reading LPS22HB using the same driver as ST is giving. I always read the same value of pressure i.e 1847. Temperature value is also incorrect as it is very small.  here is code snippet from the LPS22HB_Init()   /* Make LPS22HB Reset and Reboot */… (Show more)
in MEMS and Sensors Forum
Dayananda KT
Hi ,   I am using LSM9ds1 in one of my project. The main reason for using this chip is,  it is THE one recommended for IMU feature, where all 3 sensors are in one chip.   In Android 6.0 , I am getting all 3 sensors data , Accelerormeter , Gyro and Magnetic sensor.   My question is : 1: How do I validate the IMU feature?  2: Is there any… (Show more)
in MEMS and Sensors Forum
Jason Hendrix
I believe I've configured my system (LSM6DSMTR connected to Nordic nRF52382 via I2C) to interrupt on INT2 when the FIFO threshold is reached.  What is happening, is that I get an interrupt when data first appears in the FIFO (status shows 3 samples), then after a while, I get the FTH interrupt with the status showing the FTH number of samples.  I… (Show more)
in MEMS and Sensors Forum
Arpan Patel
Hi, I have configured accelerometer's registers as follows. So, from the activity threshold value how I know that at which raw value of X, Y, and Z axis it will be interrupted on a specific pin? /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// response… (Show more)
in MEMS and Sensors Forum
Rocne Scribner
Hi everyone,   I'm working with a LIS3DH accel and having trouble reading registers. I'm able to successfully read the value from any single register, but all subsequent reads return the same value. I.e. if I read WHO_AM_I register, and then read CTRL_REG1, both read commands return the value from the WHO_AM_I register.   Has anyone encountered… (Show more)
in MEMS and Sensors Forum
niccolò ruffini
hi everyone, i'm trying to debug my program on the iNEMO M1 but when i press the reset button to start the program the iNEMO is disconnected from the debugger and i can't talk to it anymore, so i can't see where the problem is.   hardware situation: i'm using the iNEMO M1 mounted on a home-made board, programmed by the STlink of a nucleo… (Show more)
in MEMS and Sensors Forum
vasilenko.sergey
In the datasheet say that this pin must be work(indicate moment of magnetometer new data avalaible ) automatically(without need of configuration), but it doesn't work. Why? In the http://www.st.com/resource/en/datasheet/iis2mdc.pdf said that M_XYZ_DA status bit must be connected with DRDY_M output pin(page 32, CFG_REG_C (62h) 0 bit). Does not… (Show more)
in MEMS and Sensors Forum
Arpan Patel
Hello Miroslav, I have done following configuration for IIS2DH acceleromenter. /////////////////////////// Sample Code //////////////////////////////////////////////////// response=LIS3DH_GetWHO_AM_I(&who_am_i); if(who_am_i==IC_READ_SUCCESS){ print("Who AM I %x\r\n",who_am_i); unsigned char response,status; AxesRaw_t data; response =… (Show more)
in MEMS and Sensors Forum
stefan schoenbauer
I have configured the Wake-Up interrupt (with highpass filter) as described in the application note:   1. Write 60h to CTRL1_XL // Turn on the accelerometer // ODR_XL = 416 Hz, FS_XL = 2 g 2.Write 90h to TAP_CFG // Enable interrupts and apply high-pass digital filter; latched mode disabled 3.Write 00h to WAKE_UP_DUR  // No duration 4.Write 02h… (Show more)
in MEMS and Sensors Forum
Load more items