2009-02-17 4:20 PM
Use of the external trigger to initiate single ADC conversions
2011-05-17 3:42 AM
I am trying to do a simple A/D conversion, but time-synchronized to another event. For this purpose I use ADC1, regular channel, single conversion mode with an external trigger from TIM1 CC3. I perform the following procedure:
1. Turn ADC1 on (ADON bit=1) 2. Set single conversion (CONT=0) 3. Select TIM1 CC3 as the trigger (EXTSEL=010) 4. Produce these triggers at a rate of 100 kHz (confirmed by oscilloscope) 5. Set External trigger mode (EXTTRIG=1) The result is: NOTHING. The SRTR flag never comes on. The EOC flag never comes on. No data is in ADC_DR. While messing around with this I discovered that a conversion will occur the second time I set the EXTTRIG bit to 1, even though it is already 1. It appears to be analagous to the use of the ADON bit to trigger a conversion from software (you need to set it to 1 to turn the ADC on, then write a 1 to it again to start a conversion). This is documented in the Programmer's guide for the ADON bit, but I can find no mention of a similar behavior for the EXTTRIG bit. Also I have determined that when I set the EXTTRIG to 0, then the next time I set it to 1, no conversion occurs. A second write to the bit is always necessary. But if I never reset it to 0, then a conversion will occur each time I write a 1. Can anyone confirm that this is how it is supposed to work? When the EXTTRIG is set to 1 and a contiuous stream of triggers is sent out (the rate in my application is 100 kHz), will the ADC perform exactly one conversion and then stop, or will it perform a conversion every time it gets a trigger? Paul Cornelius2011-05-17 3:42 AM
Paul -
Did you ever get an answer for this? I have hit the same screen. Am trying to trigger off of a periodic TIM2_CC2 event. I can see the timer event on both a scope and the debugger. But can seem to configure the ADC to recognize the trigger. Grateful for any input, - Bill2011-05-17 3:42 AM
Bill:
No one ever replied, and I ended up doing things a different way. But if I remember correctly, I had to set the EXTTRIG flag twice in order to get the first conversion to occur, and set it again for each A/D conversion I wanted to perform thereafter. It seemed like each time I set the bit to 1 the ADC became ''armed'' for one conversion. I didn't verify that these conversions were in fact initiated by the hardware trigger, but I assume that they were. So I think after each conversion, you will need to move the data out of the result register and then re-arm the ADC with another EXTTRIG=1. Paul Cornelius2011-05-17 3:42 AM
Guys,
That's horrendous, and completely defeats the usefulness of DMA to fill a buffer from the ADC. Seriously, is there no way to use DMA to transfer conversion results when the ADC is using an external trigger? Does it only work for; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ??? Did anyone ask ST tech support about this? James.2011-05-17 3:42 AM
After reading the code offered in this thread
I adapted mine to use timer 3 instead of 1. Also the example.c kindly posted uses; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T3_TRGO; and TIM_SelectOutputTrigger(TIM3, TIM_TRGOSource_Update); With these changes, I *think* I have it working as desired now. Cheers, James.