2021-04-07 9:10 AM
Hello!
I'm trying to use an external SDRAM (IS42S16320F) with an STM32H753 but no luck till now.
Could please anyone check if my settings are correct because I don't know if I made a bug here.
For that I have attached the FMC configuration and the schematic parts with the SDRAM and uC.
I would be very greatefull for that.
Regards,
Gregor
2021-04-08 11:42 AM
Hi!
Here some update for the topic.
I was trying to change the refresh rate according to the proposal to 400:
#define REFRESH_COUNT ((uint32_t)0x0190) /* SDRAM refresh counter (100Mhz SD clock) */
which is set by the last step in the initialization function:
/* Step 6: Set the refresh rate counter */
/* Set the device refresh rate */
HAL_SDRAM_ProgramRefreshRate(hsdram, REFRESH_COUNT);
that runs this one:
HAL_StatusTypeDef FMC_SDRAM_ProgramRefreshRate(FMC_SDRAM_TypeDef *Device, uint32_t RefreshRate)
{
/* Check the parameters */
assert_param(IS_FMC_SDRAM_DEVICE(Device));
assert_param(IS_FMC_REFRESH_RATE(RefreshRate));
/* Set the refresh rate in command register */
MODIFY_REG(Device->SDRTR, FMC_SDRTR_COUNT, (RefreshRate << FMC_SDRTR_COUNT_Pos));
return HAL_OK;
}
So it should set the SDRTR register to the value 0x0190.
After setting a breakpoint just after this function, the register has a value of 0x0:
Now I' checking why this is so, but this dosen't supose to look like this...
2021-04-09 11:33 AM
Hello!
I have found the problem. The reason, why the register was not set, was very easy: I forgot to change in the SDRAM initialization function the number of the SDRAM to 2 (since I'm using the SDRAM2).
You can see here the sdramHandle is set to hsdram2 and everything works fine :)
void BSP_SDRAM_Init(void)
{
sdramHandle = hsdram2;
/* Program the SDRAM external device */
SDRAM_Initialization_Sequence(&sdramHandle, &command);
}
/**
* @brief Perform the SDRAM external memory inialization sequence
* @param hsdram: SDRAM handle
* @param Command: Pointer to SDRAM command structure
* @retval None
*/
void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Command)
{
__IO uint32_t tmpmrd =0;
/* Step 1: Configure a clock configuration enable command */
Command->CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;;
Command->AutoRefreshNumber = 1;
Command->ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, Command, SDRAM_TIMEOUT);
I have checked the registers and they are set now correctly.
I also wrote a simple code to do a first test:
The result is fine in memory view and variable check:
Thank you all for all the help!
Now I can continue to write my test code.
Regards,
Gregor