2012-08-01 9:11 AM
Hi All,
I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3240 eval board, and works really fine. Can someone help me?? Have someone find (and solved) the same problem?? I will really appreciate some answer, because a don't know what more to do... Thanks in advance!!2012-08-01 11:18 AM
I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3240 eval board, and works really fine.
So not a software issue then, how about on a reference design using the SMSC part? Providing a snap shot of your schematic might provide for more informed discussion.2012-08-09 5:12 AM
You're not the only one. See thread 'STM32F2/F4 problams with various ULPI USB PHYs'
You can find it by seaching forums for ChirpK.RegardsIan