2023-05-27 1:33 PM
I have an Adafruit STM32F405 Feather Express. I am compiling / uploading with Arduino IDE V2.1.0 with Windows 11 64. The board worked well for about a week, but no longer connects/shows up as Port 5 of USB. I was successfully connecting and uploading code with the Arduino IDE. After a few days away from the project, I discovered my STM32F405 Express no longer connects to the USB. I did attempt to install MS WDAC - see below.
When I jump B0 to +3.3 and press reset, (I hear a USB connect sound) under "Universal Serial Bus devices", "STM BOOTLOADER" appears in the device manager; it's always visible w/ or w/o the 405 if "View -> Show hidden devices" is checked). Unplugging the USB after a BO+reset generates a "disconnect" sound. Nothing appears under "Ports (COM & LPT)". When it was working, I could see it under "Port 5". Now, neither the STM32, nor any other device, is visible on the IDE under "Tools -> Port".
With the device manager and looking the STM BOOTLOADER Device Manager properties / Events tab / "Device install requested", I see "Device USB\VID_0483&PID_DF11\2065326F4D31 requires further installation." A B0+reset generates a "connect" sound, but no sound is generated otherwise.
The code I previously uploaded which simply sets up two PWM channels appears to be working - I can see waveforms on the 6 and 9.
If I connect a Nano to the USB, "USB-SERIAL CH340 (COM6)" appears and the Arduino IDE sees it as "COM6".
After seeing a caution icon on the "Windows Security - Actions recommended" icon in the task bar, I did attempt, apparently unsuccessfully, to install the Microsoft Windows Defender Application Control about the time the problem occurred. MS WDAC.
I did uninstall/reinstall Arduino IDE 2.1.0 The problem still exists. Same content in the Device Manager. Uninstalled/reinstalled "STM32 MCU based boards by STMMicroelectronics" 2.5.0 Per the instructions on Arduino IDE Setup setup page, "STM32 Cores by STMicroelectronics" no longer appears to exist, used a new version.
Any suggestions or hints would be appreciated.
Thanks -Jim
Edit: Adding the Event Viewer log
=============================================================
Installation configuration
Level: Information
time stamp: 5/27/2023 13:03:45
=============================================================
Device USB\VID_0483&PID_DF11\2065326F4D31 was configured.
Driver Name: oem180.inf
Class Guid: {88bae032-5a81-49f0-bc3d-a4ff138216d6}
Driver Date: 05/07/2018
Driver Version: 1.1.0.0
Driver Provider: STMicroelectronics
Driver Section: USB_Install
Driver Rank: 0xFF0001
Matching Device Id: USB\VID_0483&PID_DF11
Outranked Drivers:
Device Updated: false
Parent Device: USB\VID_045B&PID_0209\6&38487f98&0&1
=============================================================
Level: Error.
Time stamp: 5/27/2023 13:03:45
Device USB\VID_0483&PID_DF11\2065326F4D31 had a problem starting.
=============================================================
Driver Name: oem180.inf
Class Guid: {88bae032-5a81-49f0-bc3d-a4ff138216d6}
Service: WinUSB
Lower Filters:
Upper Filters:
Problem: 0x0
Problem Status: 0xC00000E5
2023-06-08 3:38 PM
Got it working! I deleted C:\Users\...\AppData\Local\Arduino15\packages\stm32duino and C:\Users\...\AppData\Local\Arduino15\packages\STMicroelectronics then reloaded.
2023-06-08 5:23 PM
Could STM32 Cube Programmer not see/use the "STM32 BOOTLOADER" device?
2023-06-08 5:59 PM
Attempting to install Microsoft's Vulnerable Driver Blocklist was the only thing I think might have done it. It was working fine, I took a break for a few days. During that break, I installed. A few days later, I tried to connect and it no longer worked.