2017-10-25 12:34 PM
I have the USB HID demo working on an STM32F072B-DISCO board. I grabbed the code from the HID demo app to make a custom Windows project. Everything works alright, but I want to increase the report length (the demo report length is 2). I changed the HID_IN_PACKET and HID_OUT_PACKET macros to 64. After my device enumerates, USB Viewer shows the wMaxPacketSize as 64 as expected. However, the HIDP_CAPS InputReportByteLength and OutputReportByteLength in my Windows app are still reporting lengths of 2.
How do I increase the input and output report lengths in the demo application?
Solved! Go to Solution.
2017-10-26 4:43 PM
I figured it out.
I needed to increase the report number, report size, and maximum logical value in my report description.
2017-10-26 4:43 PM
I figured it out.
I needed to increase the report number, report size, and maximum logical value in my report description.