2009-03-06 03:38 AM
USB host with STM32F105Rx shematic
2011-05-17 04:05 AM
Hello,
how can I connect the USB port to the STM32F105Rx controller if I need USB host support. How are the OTG_FS_SOF, OTG_FS_ID and OTG_FS_ID signals used. Can someone give me a description of this signals. My USB port supply is driven by a TPS 2051 port switch with has a over current detection output. Is the detection connected to a GPIO input PIN ? Are there any application notes or infos about USB host with this controller. Thanks for your help.