cancel
Showing results for 
Search instead for 
Did you mean: 

USB host with STM32F105Rx shematic

bjoern
Associate
Posted on March 06, 2009 at 12:38

USB host with STM32F105Rx shematic

1 REPLY 1
bjoern
Associate
Posted on May 17, 2011 at 13:05

Hello,

how can I connect the USB port to the STM32F105Rx controller if I need USB host support.

How are the OTG_FS_SOF, OTG_FS_ID and OTG_FS_ID signals used. Can someone give me a description of this signals. My USB port supply is driven by a TPS 2051 port switch with has a over current detection output. Is the detection connected to a GPIO input PIN ? Are there any application notes or infos about USB host with this controller.

Thanks for your help.