2014-11-06 12:21 AM
i'm using f407zg and try to use USB HS host with internal PHY but found the program never entry interrupt function
my program is modify form host_device_libV2.10-USB_host_example which i tried on eval board successfullyi already defined USE_EMBEDDED_PHY marco and there are init code: USBH_Init(&USB_OTG_Host, USB_OTG_HS_CORE_ID, &USB_Host, &USBH_MSC_cb, &USR_Callbacks);void USB_OTG_BSP_Init(USB_OTG_CORE_HANDLE *pdev){ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOB , ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15 | GPIO_Pin_14; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB,GPIO_PinSource15,GPIO_AF_OTG2_FS) ; GPIO_PinAFConfig(GPIOB,GPIO_PinSource14,GPIO_AF_OTG2_FS) ; RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ;}so any advice?2014-11-06 3:59 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/USB%20host%20problem%202194&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=6]Duplicate Thread
Regards,Heisenberg.2014-11-09 9:53 PM
Sorry, how to delete that thread?
and...any help?2014-11-11 7:29 PM
anyone anyhelp?