2014-02-28 7:50 AM
i use stm32f4 discovery board with keil ide.
but i can't know from where i can start with stm32 . '' i was use usb with pic microchip '' i just want transfer data between pc and stm32f4 using usb.2014-02-28 8:06 AM
Hi
''i use stm32f4 discovery board .'' Is the board you are talking about this one : http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF252419 '' i want to use usb'' '' i just want transfer data between pc and stm32f4'' HID = Human interface device (eg mouse, keyboard or joystick) CDC = serial comms device (eg virtual RS232) MSC = Mass Storage Device (eg memory stick) CDC is probably the easiest. On the link above - look under ''Related Tools and Software'' ''STM32F4DISCOVERY board firmware package, including 22 examples (covering USB Host, audio, MEMS accelerometer and microphone) (AN3983)
'' Should have some examples for USB devices2014-03-01 11:05 AM
thank you
yes i have this board in your link. ''STM32F4DISCOVERY board firmware package, including 22 examples (covering USB Host, audio, MEMS accelerometer and microphone) (AN3983)
'' i already have this file . and it's use usb host and it's not easy and not why i want. cdc are i have usb to rs232 convertter chip i want to connect stm32 with usb not rs232.2014-03-03 1:44 AM
Hi
''i already have this file . and it's use usb host and it's not easy and not why i want. cdc are i have usb to rs232 convertter chip i want to connect stm32 with usb not rs232.'' Here is the library code for USB : www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882 It should contain examples of USB devices (including USB CDC - serial device). The examples are for the range of processors (not specific for your board). (I think the CDC example also mixes USB CDC with the USART)