2009-03-05 03:39 AM
USB HID Demonstrator Source Code
2011-05-17 04:05 AM
Is the USB HID Demonstrator Source Code available somewhere? Couldn't find it yet.
I also read somewhere in the forum, that STM couldn't publish it because it includes some 3rd party graphic components (they were talking about an older version, though). However, I'm more interested in the functionality. Wouldn't it be possible to release a community version without the 3rd party graphic components. I'd appreciate it. -Stefan2011-05-17 04:05 AM
Hi Stefan,
All sources files are available on web http://www.st.com/stonline/products/support/micro/files/um0551.zip After installation, you will find them in ''C:\Program Files\STMicroelectronics\Software\USB HID Demonstrator\src'' sub-directory if you do not change the default installation. BTW, I do not know from where you get that '' STM couldn't publish it because it includes some 3rd party graphic components'' :| , Anyway, I let you enjoy them 🙂 Cheers, STOne-32.2011-05-17 04:05 AM
Thanks for the link.
I found that comment there: Although, after reading over it again I noticed that the ''we can't distribute them'' was related to the 3rd party apps and not the source code (which is actually attached). My fault, sorry.