2017-02-20 3:37 AM
Hello,
can the information be made available how the on-chip USB bootloader generates the serial number?
This would be helpfull when an application provides a DFU endpoint to jump to the built-in USB bootloader. As long as the application does not know how to generate the same serial number as the bootloader, the DFU application needs to know both serial numbers and both numbers need to be provides by the user.
Thanks
2017-02-23 8:48 AM
Hello
Bonnes.Uwe
,The serial number is generated from the UID (3 words) of the chip combined as following:
Sum of first and third words used
Second word not modified
It will be better to provide more details about your casein order
to help you achieve your goal:
What you want to do ? Do you want
enumerate DFU from flash then jumps to Bootloader ?
Regards
Imen
2017-02-24 8:02 AM
,
,
Hello,
with appended code I can reproduce the Bootloader Serial for F3 and F4:
extern char serial_no[13],
♯ if defined(UID_BASE)
,
uint16_t *uid_base = (uint16_t *)UID_BASE,,
sprintf(serial_no, '%04X%04X%04X', uid_base[1] + uid_base[5], uid_base[0] + uid_base[4],,
♯ if defined(MCU_STM32F3),
, , , uid_base[5]), /* 5 fits for F3*/,
♯ else,
, , , uid_base[3]), /* 3 fits for F4*/,
♯ endif,
♯ else,
serial_no[0] = 0,,
♯ endifIt seems F3 and F4 have slight differences!
2017-03-16 12:38 AM
DFU serial number
STM32F2, STM32F4: 8 hex digits of (UID0 + UID2) followed by 4 hex MSB digits of (UID1)
UID 012: 002d0030 3334510b 32313533
SerialNumber: 325E35633334
STM32F3: 8 hex digits of (UID0 + UID2) followed by 4 hex MSB digits of (UID2)
UID 012: 003b0041 50335706 20333333
SerialNumber: 206E33742033