Usart4 no TX
Hi Forum,
I'm using the stm32f091RCt6, (LQFP64) to set up USART4
Kind Regards
Bob
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // Enable GPIOC clock RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); // Enable USART3 APB clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART4, ENABLE); // Connect pin to Periph GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_0); // USART4 TX GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_0); // USART4 RX // Configure pins as AF pushpull GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOC, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART4, &USART_InitStructure); USART_Cmd(USART4, ENABLE); // Enable the COM4 Receive interrupt: this interrupt is generated when the// COM4 receive data register is not empty USART_ITConfig(USART4, USART_IT_RXNE, ENABLE);// USART4 IRQ Channel configuration
NVIC_InitStructure.NVIC_IRQChannel = USART3_8_IRQn;NVIC_InitStructure.NVIC_IRQChannelPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);Although I can receive data I cannot get any TX at all. I have usart1 and usart2 working fine. not sure what is is. I've buzzed out all the board connections and they are fine. Looking at the clock tree on page16 of the datasheet, I notice PCLK only goes to usart1, usart2 and usart3. Does usart4 need some aqlternative form of clocking? The datasheet really doesnt say to much about usarts4 to 8 and there are no app notes out there to refer to so i'm stuck at this point.
Thanks for any help.
Regards Bob