2014-08-14 2:05 AM
Hello All
I am working on STM32F429 with TFT and using DISCOVERY DISCO board Trying to use 2 UARTS ->>>> UART1 and UART 4 or 6 UART4 with PA0 and PA1 pins PA0 is tied to switch but it should show some activity. No Tx or Rx is working whereas same thing work fine on USART 1 Able to run UART1 and is working fine but nor any other! I am using real-term console for this experiment and have leds on my USB to serial for displaying any activity. its really frustrating..... Following is my code May be i am doing some thing wrong
1.
//***************************** USART_SETUP *******************************<br>void USART_SETUP(void)<br>{<br> GPIO_InitTypeDef GPIO_InitStructure;<br> USART_InitTypeDef USART_InitStruct;<br> <br> RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);<br> RCC_APB2PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);<br>// RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);<br> RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);<br> /*<br><br><br> -------------------------- USART1 ---------------------------<br> PA9 is USART1_TX<br> PA10 is USART1_RX<br><br><br>xxxxxxxxxxx PB6 is USART1_TX<br> PB7 is USART1_RX<br><br><br> -------------------------- USART2 ---------------------------<br> PA2 is USART1_TX<br>xxxxxxxxxxx PA3 is USART1_RX<br> <br> PD5 is USART1_TX<br>xxxxxxxxxxx PD6 is USART1_RX<br> <br> -------------------------- USART3 ---------------------------<br>xxxxxxxxxxx PB10 is USART1_TX<br>xxxxxxxxxxx PB11 is USART1_RX<br> <br>xxxxxxxxxxx PC10 is USART1_TX<br> PC11 is USART1_RX<br> <br>xxxxxxxxxxx PD8 is USART1_TX<br>xxxxxxxxxxx PD9 is USART1_RX<br><br><br> -------------------------- USART4 ---------------------------<br> PA0 is USART1_TX<br> PA1 is USART1_RX<br> <br>xxxxxxxxxxx PC10 is USART1_TX<br> PC11 is USART1_RX<br> <br> -------------------------- USART5 ---------------------------<br> PC12 is USART1_TX<br> PC2 is USART1_RX<br> <br> -------------------------- USART6 ---------------------------<br>xxxxxxxxxxx PC6 is USART1_TX<br>xxxxxxxxxxx PC7 is USART1_RX<br> <br> PG14 is USART1_TX<br> PG9 is USART1_RX<br> <br> -------------------------- USART7 ---------------------------<br>xxxxxxxxxxx PE8 is USART1_TX<br>xxxxxxxxxxx PE7 is USART1_RX<br> <br> PF7 is USART1_TX<br> PF6 is USART1_RX<br> <br> -------------------------- USART8 ---------------------------<br>xxxxxxxxxxx PE1 is USART1_TX<br>xxxxxxxxxxx PE0 is USART1_RX<br> */ <br><br><br>/////// Configure USART1 Rx (PA10) as input<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; <br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOA, &GPIO_InitStructure);<br><br>/////// Configure USART1 Tx (PA9) as alternate function<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;<br> GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;<br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOA, &GPIO_InitStructure); <br> <br> GPIO_PinAFConfig(GPIOA,GPIO_PinSource9,GPIO_AF_USART1);<br> GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_USART1);<br><br><br><br><br> <br> // Configure UART4 Rx (PA1) as input<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; <br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOA, &GPIO_InitStructure);<br><br> // Configure UART4 Tx (PA0) as alternate function<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;<br> GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;<br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOA, &GPIO_InitStructure); <br> <br> GPIO_PinAFConfig(GPIOA,GPIO_PinSource0 ,GPIO_AF_UART4);<br> GPIO_PinAFConfig(GPIOA,GPIO_PinSource1 ,GPIO_AF_UART4);<br> <br> <br> <br> <br> <br> // Configure USART6 Rx (PG9) as input<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; <br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOG, &GPIO_InitStructure);<br><br> // Configure USART6 Tx (PG14) as alternate function<br> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;<br> GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;<br> GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;<br> GPIO_Init(GPIOG, &GPIO_InitStructure); <br> <br> GPIO_PinAFConfig(GPIOG,GPIO_PinSource9 ,GPIO_AF_USART6);<br> GPIO_PinAFConfig(GPIOG,GPIO_PinSource14,GPIO_AF_USART6);<br> <br> /* USARTx configured as follow:<br> - BaudRate = 9600 baud <br> - Word Length = 8 Bits<br> - One Stop Bit<br> - No parity<br> - Hardware flow control disabled (RTS and CTS signals)<br> - Receive and transmit enabled<br> */<br> USART_InitStruct.USART_BaudRate = 57600;<br> USART_InitStruct.USART_WordLength = USART_WordLength_8b;<br> USART_InitStruct.USART_StopBits = USART_StopBits_1;<br> USART_InitStruct.USART_Parity = USART_Parity_No;<br> USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;<br> USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;<br> USART_Init(USART1, &USART_InitStruct);<br><br><br> USART_InitStruct.USART_BaudRate = 9600;<br> USART_InitStruct.USART_WordLength = USART_WordLength_8b;<br> USART_InitStruct.USART_StopBits = USART_StopBits_1;<br> USART_InitStruct.USART_Parity = USART_Parity_No;<br> USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;<br> USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;<br> USART_Init(UART4, &USART_InitStruct);<br><br><br> USART_Cmd(USART1, ENABLE);<br> USART_Cmd(UART4, ENABLE);<br>}<br><div></div>
#stm32f429discovery #uart4
2014-08-14 3:40 AM
Code in normal format
//***************************** USART_SETUP *******************************void USART_SETUP(void){ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStruct; RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);// RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* -------------------------- USART1 --------------------------- PA9 is USART1_TX PA10 is USART1_RXxxxxxxxxxxx PB6 is USART1_TX PB7 is USART1_RX -------------------------- USART2 --------------------------- PA2 is USART1_TXxxxxxxxxxxx PA3 is USART1_RX PD5 is USART1_TXxxxxxxxxxxx PD6 is USART1_RX -------------------------- USART3 ---------------------------xxxxxxxxxxx PB10 is USART1_TXxxxxxxxxxxx PB11 is USART1_RX xxxxxxxxxxx PC10 is USART1_TX PC11 is USART1_RX xxxxxxxxxxx PD8 is USART1_TXxxxxxxxxxxx PD9 is USART1_RX -------------------------- USART4 --------------------------- PA0 is USART1_TX PA1 is USART1_RX xxxxxxxxxxx PC10 is USART1_TX PC11 is USART1_RX -------------------------- USART5 --------------------------- PC12 is USART1_TX PC2 is USART1_RX -------------------------- USART6 ---------------------------xxxxxxxxxxx PC6 is USART1_TXxxxxxxxxxxx PC7 is USART1_RX PG14 is USART1_TX PG9 is USART1_RX -------------------------- USART7 ---------------------------xxxxxxxxxxx PE8 is USART1_TXxxxxxxxxxxx PE7 is USART1_RX PF7 is USART1_TX PF6 is USART1_RX -------------------------- USART8 ---------------------------xxxxxxxxxxx PE1 is USART1_TXxxxxxxxxxxx PE0 is USART1_RX */ /////// Configure USART1 Rx (PA10) as input GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOA, &GPIO_InitStructure); /////// Configure USART1 Tx (PA9) as alternate function GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA,GPIO_PinSource9,GPIO_AF_USART1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_USART1); // Configure UART4 Rx (PA1) as input GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOA, &GPIO_InitStructure); // Configure UART4 Tx (PA0) as alternate function GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA,GPIO_PinSource0 ,GPIO_AF_UART4); GPIO_PinAFConfig(GPIOA,GPIO_PinSource1 ,GPIO_AF_UART4); // Configure USART6 Rx (PG9) as input GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOG, &GPIO_InitStructure); // Configure USART6 Tx (PG14) as alternate function GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOG, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOG,GPIO_PinSource9 ,GPIO_AF_USART6); GPIO_PinAFConfig(GPIOG,GPIO_PinSource14,GPIO_AF_USART6); /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStruct.USART_BaudRate = 57600; USART_InitStruct.USART_WordLength = USART_WordLength_8b; USART_InitStruct.USART_StopBits = USART_StopBits_1; USART_InitStruct.USART_Parity = USART_Parity_No; USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStruct); USART_InitStruct.USART_BaudRate = 9600; USART_InitStruct.USART_WordLength = USART_WordLength_8b; USART_InitStruct.USART_StopBits = USART_StopBits_1; USART_InitStruct.USART_Parity = USART_Parity_No; USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStruct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(UART4, &USART_InitStruct); USART_Cmd(USART1, ENABLE); USART_Cmd(UART4, ENABLE);}2014-08-14 5:12 AM
Please don't [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Multiple%20UART%20Problem%20%21%20%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=7]cross-post, and use the Code Format Block tool (Paintbrush [<>] icon, upper left)