USART1 with STM32F0 Discovery
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-22 8:14 AM
Dear All,
I write a program for USART1 of STM32F0 Discovery board. I am sure that my hardware is working . I configured with PuTTY but it does not display the message Please advice PA10 RX to MAX 232 pin 12 PA9 TX to MAX 232 pin 11#include ''stm32f0xx.h''
#include ''stm32f0xx_tim.h''
#include <
stm32f0xx_rcc.h
>
#include ''stm32f0xx_usart.h''
void gpio_init(){
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd (RCC_AHBPeriph_GPIOC | RCC_AHBPeriph_GPIOA,ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_8 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void LED(){
GPIOC->ODR ^= GPIO_Pin_8;
}
void USART_gpio_Initialize(){
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0);
//Configure USART1 pins: Rx and Tx ----------------------------
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
void USART_Initialize(){
//Configure USART2 setting: ----------------------------
USART_InitTypeDef USART_InitStructure;
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1,ENABLE);
}
void Send_Data(){
while(1) {
while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
USART_SendData(USART1, 'A');
}
}
int main(){
gpio_init();
LED();
USART_gpio_Initialize();
USART_Initialize();
Send_Data();
//while(1){}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-22 8:38 AM
RCC_APB1PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
APB2 not APB1
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-22 9:01 AM
Dear Sir,
Great thanksI changed the code, bit problem is remaining the same RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);please advice- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-22 1:01 PM
Do you have an oscilloscope? Can you confirm the bit timing with that?
The primary issue with serial baud rates on STM32 devices is the incorrect configuration of HSE_VALUE, this define must match the clock rate of the externally supplied clock if that is used. I'm not going to look up MAX232 datasheets, but what voltage are you using, as I recall the MAX232 is not 3V compatible, perhaps thehttp://www.maximintegrated.com/en/datasheet/index.mvp/id/1068
? Can you receive data on the STM32 if you loop back TX to RX, on either the current USART, or a second one? Are there any other connections to USART1 on the STM32F0-DISCO board, review the schematic, check if it goes to the ST-LINK device.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-23 7:52 AM
Do you have an oscilloscope? Can you confirm the bit timing with that?
Sorry I should not haveThe primary issue with serial baud rates on STM32 devices is the incorrect configuration of HSE_VALUE, this define must match the clock rate of the externally supplied clock if that is used.
I am using default internal clock ofSTM32F0DISCOVERY (STM32F051R8T6) kitCan you receive data on the STM32 if you loop back TX to RX
Yes.loop-backis working for second one ( Hardware USART)Are there any other connections to USART1 on the STM32F0-DISCO board
As per the attached schismatic it does not have connected with others ________________ Attachments : STM32F0DISCOVERY_Hardware_and_layout.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0P1&d=%2Fa%2F0X0000000bb7%2FZb_yDjXy5HkhIvUJpAnORGHnVPrL6hGEhC7KUgDbxxw&asPdf=false- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-23 9:08 AM
Please don't attach publicly available documents to the forum, cite a link if you must refer to them. The task to review the schematic is yours, not really mine.
A complete schematic of what circuitry you've attached, that might be salient, as I wouldn't have access to that. Absent a scope you'll need to confirm the clocks, signals and voltages. Perhaps you can use the GetClocks api and sprintf to a buffer, and view that buffer in the debugger?Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-24 9:29 AM
Dear Sir,
Grate thanks for the advice Now my program is workingThe issue was GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0
);GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0
);But it should be GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1
); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1
);AF_0 should be AF_1But my question is as per the stm32f0xx.gpio.h the GPIO_Alternate_function_selection_define @brief AF 0 selection */#define GPIO_AF_0 ((uint8_t)0x00) /* WKUP, EVENTOUT, TIM15, SPI1, TIM17, MCO, SWDAT, SWCLK, TIM14, BOOT,USART1
, CEC, IR_OUT, SPI2 */Please adviceThanks in advance- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-24 12:35 PM
On the PB6/7 pins USART1 is AF0, the Data Sheet should be the controlling document here.
One of the issues is that the F0 design has the pin mux design optimized to use the least amount of silicon, rather than say the F4 where more consistency is applied to the mux numbering across peripherals, but having more unused gaps.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-24 11:31 PM
Dear Sir,
Thanks for the replyI configured the USART1 for pin PB6 - PB7 and it is working but stranger is it does care about following codes GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_0); GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_0);It is working without above codes- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-25 8:55 AM
Probably because the reset setting of the bits related to the AF Mux are zero.
Up vote any posts that you find helpful, it shows what's working..