cancel
Showing results for 
Search instead for 
Did you mean: 

USART problem

piotr2
Associate
Posted on February 17, 2014 at 14:24

Hi!

I tried to establish USART connection between my STM32F103RB with PC and I cannot do it. I searched many topics and forums and tried different possiblities and nothing worked.

I also tried to make a USART connection on my board (between USART1 and USART2) and it worked fine. Unfortunately after rewiring cables to connect USART1 with ZL4USB (this is board with opto-isolation using FT232R) I send and receive some rubbish.

I'd be grateful for getting some help.

#usart-stm32
13 REPLIES 13
Posted on February 23, 2014 at 03:17

While that might be possible, I suspect the reason for it not working is much more mundane.

Off by one, or PA9/PA10 reversed?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pafshan
Associate II
Posted on February 23, 2014 at 04:55

Attached is the schematic of the circuit. I checked the PA9 and PA10 and even exchanged them just to see. But no response from the terminal at all.

Many thanks!

________________

Attachments :

scan0001.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0bi&d=%2Fa%2F0X0000000bb8%2FirCmfVn6Pyi3UgaEHJalov8Yzt_taZ4XITLeq5FC328&asPdf=false
Posted on February 23, 2014 at 14:38

Ok, reasonable. Is the serial the same arrangement you tested with the VL-Discovery?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pafshan
Associate II
Posted on February 23, 2014 at 18:03

Yes, everything is exactly the same as the VL-discovery except the board.

Any initialization is needed for a brand new chip?