Posted on February 23, 2014 at 18:03Yes, everything is exactly the same as the VL-discovery except the board.Any initialization is needed for a brand new chip?
Posted on February 23, 2014 at 04:55 Attached is the schematic of the circuit. I checked the PA9 and PA10 and even exchanged them just to see. But no response from the terminal at all. Many thanks!
________________
Attachments : scan000...
Posted on February 23, 2014 at 02:46I will make the schematics and send to you shortly.One thing I forget to mention: I purchased the proto board and solder the chip on it myself. Instead of reflowing it, I used my solder iron and tap-soldering all ...
Posted on February 22, 2014 at 19:34Clive1,Thanks for your help. The VDDA is connected to the 3.3V and the NRST pin is put on momentary low at reset.However when I issued 7f (and 0x7f since I am not sure what is the correct format) at the RealTerm, ...
Posted on February 22, 2014 at 05:28I am new to this forum and also new to the STM32f100 uC.I recently bought two STM32f100 value line discovery boards and am able to program it for some simple functions. I can download the code to the flash memory ...