2013-10-28 10:00 AM
Hi Folks,
I am a little bit confused about the USART built in in the STM32F051. He is don`t talking to me although I am asking really polite. This is my init-code: RCC -> AHBENR |= (RCC_AHBENR_GPIOAEN); //PA9 GPIOA->OSPEEDR |= (1UL<< 18); //MEDIUM SPEED GPIOA->OTYPER &= ~(1UL<<9); //Push-pull GPIOA->MODER |= (1UL<<19); //AF-Mode GPIOA->AFR[1] |= (1UL << 4); //AF1 selected //PA10 GPIOA->MODER |= (1UL<<21); // AF-Mode GPIOA->AFR[1] |= (1UL<<8); // AF1 selected RCC ->APB2ENR |= (1UL<<14); USART1 -> CR1 = 0x0000000C; // enable TX and RX USART1 -> CR2 = 0x00000000; USART1 -> CR3 = 0x00000000; USART1 -> BRR = 0x00000034; USART1 -> CR1 |= (1UL << 0); And this here is my TX-Routine: void USART1_tx (char TX_char){ while (!(USART1 -> ISR & ( 1UL << 6))) { __NOP();} USART1 -> TDR = TX_char; } Anyone an idea, where the problem is? #usart #stm32f0512013-10-28 10:22 AM
Anyone an idea, where the problem is?
I should care for register level code, but honestly I don't. Do you see any data on the scope? Does the baud rate look right?[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/UART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=6068]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FUART%20example%20code%20for%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=60682013-10-28 11:10 AM
Do you see any data on the scope? Does the baud rate look right?
No, on the scope is nothing. It seems to be completely dead.
2013-10-28 11:51 AM
Problem solved :-)
add this line to the code and it works. NVIC_EnableIRQ(USART1_IRQn);