2024-11-01 2:09 AM
Hi,
I am confused with pin toggle timings, why I am getting non equal pulse widths like in the picture, I turn off all compiler optimizations and disable all of the interrupts, code is simple pin toggling. My controller is STM32L431 running on 80MHz.
Thank you very much for any advice!
__disable_irq();
while(1) {
GPIOB->BSRR = GPIO_BSRR_BS15;
__NOP();
__NOP();
GPIOB->BSRR = GPIO_BSRR_BR15;
__NOP();
__NOP();
}
2024-11-01 3:21 PM
Hi,
The while(1) is NOT zero overhead. To prove it, try
__disable_irq();
while(1) {
GPIOB->BSRR = GPIO_BSRR_BS15;
__NOP();
__NOP();
GPIOB->BSRR = GPIO_BSRR_BR15;
__NOP();
__NOP();
GPIOB->BSRR = GPIO_BSRR_BS15;
__NOP();
__NOP();
GPIOB->BSRR = GPIO_BSRR_BR15;
__NOP();
__NOP();
}
I hope that helps.
Kind regards
Pedro
2024-11-02 11:29 AM
Hi PGump.1
Thank you for your reply,
unfortunatelly still uneven widths..
2024-11-02 4:02 PM
Use a simulator and step through your code at the assembly level, counting the cycles (there should a cycle count visible) - that way you will get to see the "overhead" of the loop. If you want to handcraft a loop with precise timing, you could consider doing it in assembly language.
2024-11-02 4:55 PM
@tompa wrote: "unfortunatelly still uneven widths.."
I never said it would fix it, it would prove it... Was the proof correct?
Kind regards
Pedro
2024-11-02 6:07 PM
Sampling a Nucleo-746RG @80MHz with a Saleae Logic Pro 8 at 500MS/s
Using the same code as the original post. I did not observe the significant difference in width per the first image of the post.