2025-02-17 05:52 AM
Hello everyone,
During some test I try to change the type of the StLink-V3 of the NUCLEO-H7A3ZI board to "STM32 Debug + VCP"
After this I can't flash or connect to the board even if I update back to "STM32 Debug + MAss storage + VCP".
I try to erease the flash content using STM32CubeProgrammer, after that I can connect the debugger and flash a SW :
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.070
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
The Flash succed but the target is not responding.
I also try only with a new empty project, so the SW is not the problem.
Did you have any idea how to programm again this board ?
Thanks for feedback.
Maïck
2025-02-17 06:00 AM
Hello,
Not sure what you did before that issue to occur but ensure you configured the correct power supply in SMPS. Do you confirm that?
2025-02-17 06:09 AM
Hello,
Thanks for your answer.
The only thing I do before the issue is to change the STLink firmweare.
@SofLit the supply source is configured as Direct SMPS supply
@STTwo-32 I try this procedure and after that I can flash the board but once it is flashed I get the error:
Target is not responding, retrying...