cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to calculate the correct smooth calibration value for the RTC on an STM32F411. Can you spot my error?

SORei.1
Associate II

Hello,

  I am having trouble calculating the correct calibration value for my RTC 32K osc. My setup is as follows.

STM32F411.

32768 LSE osc.

I am passing a 1HZ signal out of the micro and I am measuring it with a 5Mhz precision oscillator and counter, so if the RTC osc is perfect, I should get a count of 160,000,000 over the 32 second period.

What I actually get is a count of 159,969,776, this is a difference of 30,224 counts of 1/5mhz over a 32 second period. 

This works out to be 0.0060448 seconds out per 32 second period.

So, i need to compensate for 0.0060448 seconds using 1/32768 clock cycles.

to find out this number i divide the period by the 32k clock period (0.0060448 / (1/32768) )= 198 clock cycles. 

Because the 32768 clock is fast, i need to remove these clock cycles, so

my smooth calibration plus value = 0x00

and smooth calibration minus value = 0xc6

My problem is, when I re-measure the clock value, it is still out.

I have found that in this instance, a calibration value of 

smooth calibration plus value = 0x00

smooth calibration minus value = 0xc1

works as expected and measures to be correct.

So my assumption is, I am making a mistake in my calculation.

Can you fault anything in my method or calculation?

Thanks for reading.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

Your calculation seems to be OK, I see no reason for the difference.

Is LSE stable (i.e. are all readouts with the counter identical/close enough; after resetting RTC is the deviation still the same)? 190ppm is much more deviation than one would expect from a 32.768kHz crystal oscillator. Maybe you should start with checking your design, in particular the crystal's load capacitors. See AN2867.

JW

Piranha
Chief II

Frequency deviation of a LSE oscillator with ABS07W-32.768kHz-D-1 crystal on a two layer 1 mm board with different capacitors:

1,5 pF: +158 ppm
 15 pF: -338 ppm
4,7 pF: -104 ppm
2,7 pF:  +19 ppm
3,0 pF:  +16 ppm
3,1 pF:   +4 ppm