cancel
Showing results for 
Search instead for 
Did you mean: 

UM1851 - errors?

gbigden
Associate III
Posted on May 09, 2014 at 16:21

There seems to be a number of entries like this: 

ADC_GetCalibrationValue

Function Name uint32_t ADC_GetCalibrationValue ( ADC_TypeDef * ADCx)

Function Description Returns the ADCx calibration value.

Parameters ADCx : where x can be 1, 2, 3 or 4 to select the ADC

peripheral.

Return values None.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 22, 2014 at 18:08

Hi Gary,

Which file? Firmware package? I didn't found this UM in the web :(

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.