2014-05-09 07:21 AM
There seems to be a number of entries like this:
ADC_GetCalibrationValueFunction Name uint32_t ADC_GetCalibrationValue ( ADC_TypeDef * ADCx)Function Description Returns the ADCx calibration value.Parameters ADCx : where x can be 1, 2, 3 or 4 to select the ADCperipheral.Return values None.2014-05-22 09:08 AM
Hi Gary,
Which file? Firmware package? I didn't found this UM in the web :( -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.