cancel
Showing results for 
Search instead for 
Did you mean: 

UM0424 for V2.0 lib

ccowdery9
Associate III
Posted on June 11, 2009 at 17:55

UM0424 for V2.0 lib

3 REPLIES 3
ccowdery9
Associate III
Posted on May 17, 2011 at 13:14

I could do with an older version of UM0424 which is targetted at the V2.0 libs.

My project is built with V2.0, and I need to add some USB functionality, so it would be easier to use the older UM0424 rather than port my project up to V3.0.

Anybody know where I can get it from?

Thanks,

Chris.

ccowdery9
Associate III
Posted on May 17, 2011 at 13:14

Panic over - I found a copy locally......

Chris.

16-32micros
Associate III
Posted on May 17, 2011 at 13:14

Hi,

Be aware that we keep an archive here :

http://www.st.com/stonline/products/support/micro/files/stm32f10x_fw_archive.zip

and a patch is available to fix some limitations.

Cheers,

STOne-32.