2009-06-30 10:48 AM
polling I2C with another intrrupt
2011-05-17 4:14 AM
I use I2C2 to comunicate between STM32 and another device that his address is 0x5E .
I take the function that do read and write (in polling) from the examples of the STM32 I2C example5 . The problem is : when I enabled interrupts , after few cycles (write and read)of I2C work the I2C is stuck and dont exit from the function and all the firmware is stuck . when I disabled the interrupts it is work very good . this is the function : void I2C_Write(u8* pBuffer, u8 WriteAddr, u8 NumByteToWrite) { /* While the bus is busy */ while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY)); /* Send START condition */ I2C_GenerateSTART(I2C2, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM address for write */ I2C_Send7bitAddress(I2C2, 0x5E, I2C_Direction_Transmitter); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C2,I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C2, WriteAddr); /* Test on EV8 and clear it */ while(! I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* While there is data to be written */ while(NumByteToWrite--) { /* Send the current byte */ I2C_SendData(I2C2, *pBuffer); /* Point to the next byte to be written */ pBuffer++; /* Test on EV8 and clear it */ while (!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); } /* Send STOP condition */ I2C_GenerateSTOP(I2C2, ENABLE); } void I2C_Read(u8* pBuffer, u8 ReadAddr, u16 NumByteToRead) { /* While the bus is busy */ while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY)); /* Send START condition */ I2C_GenerateSTART(I2C2, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM address for write */ I2C_Send7bitAddress(I2C2, 0x5E, I2C_Direction_Transmitter); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C2,I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Clear EV6 by setting again the PE bit */ I2C_Cmd(I2C2, ENABLE); /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C2, ReadAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send STRAT condition a second time */ I2C_GenerateSTART(I2C2, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM address for read */ I2C_Send7bitAddress(I2C2, 0x5E, I2C_Direction_Receiver); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); /* While there is data to be read */ while(NumByteToRead) { if(NumByteToRead == 1) { /* Disable Acknowledgement */ I2C_AcknowledgeConfig(I2C2, DISABLE); /* Send STOP Condition */ I2C_GenerateSTOP(I2C2, ENABLE); } /* Test on EV7 and clear it */ if(I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_RECEIVED)) { /* Read a byte from the EEPROM */ *pBuffer = I2C_ReceiveData(I2C2); /* Point to the next location where the byte read will be saved */ pBuffer++; /* Decrement the read bytes counter */ NumByteToRead--; } } /* Enable Acknowledgement to be ready for another reception */ I2C_AcknowledgeConfig(I2C2, ENABLE); } wait to your assistant2011-05-17 4:14 AM
There are some well known issues with the STM32 and I2C.
Check out the errata (doc # 14732), section 2.9.1. Also check out this post: http://www.st.com/mcu/forums-cat-7652-23.html - Matt