cancel
Showing results for 
Search instead for 
Did you mean: 

ultrasonic A02YYUW not working in STM32L443VCT6

roystm321
Visitor

Hi,

I try to comuunicate between STM32L443VCT6  and ultrasonic A02YYUW (By UART1) 

Just to make sure that the ultrasonic is working ok, i tested it by UART1 with model: stm32 neucler f441 and everthing works ok.

 

This is the code for the STM32L443VCT6:

 

 

 

#include "main.h"
#include "string.h"
#include "stdio.h"
#include "stdlib.h"
#include <stdbool.h>

UART_HandleTypeDef huart1;

uint8_t data[4] = {0};  // Buffer to hold the 4 bytes from the sensor
float distance = 0.0;

void SystemClock_Config(void);
void MX_GPIO_Init(void);
void MX_USART2_UART_Init(void);

int main(void) {
    HAL_Init();
    SystemClock_Config();  // Use internal oscillator (MSI)
    MX_GPIO_Init();
    USART1_UART_Init();




    /* Infinite loop */
    while (1) {
      /* Wait for the start corrector (0xFF) */
      do {
        HAL_UART_Receive(&huart1, &data[0], 1, HAL_MAX_DELAY);
      } while (data[0] != 0xFF);

      /* Clear the data array before receiving new data */
      //clearDataArray();

      /* Start receiving 3 more bytes of data */
      for (int i = 1; i < 4; i++) {
        HAL_UART_Receive(&huart1, &data[i], 1, HAL_MAX_DELAY);  // Blocking receive
      }

      /* Process the sensor data */
      processSensorData();

      HAL_Delay(100);  // Delay for sensor refresh (similar to Arduino delay)
    }

    /* Infinite loop */
    while (1) {
        // Keep running if needed, or you can add additional functionality
    }
}



void processSensorData(void) {
  /* Validate the checksum */
  int sum = (data[0] + data[1] + data[2]) & 0x00FF;
 // if (sum == data[3]) {
    /* Calculate the distance */
    distance = (data[1] <<  + data[2];  // Combine the two bytes into a 16-bit value
    distance = distance / 10.0;           // Convert distance to cm

    /* Blink the LED to indicate valid data */

    if(distance<10){

    	HAL_Delay(500);
    }
 // } else {
    // Handle checksum error (optional)
  //}
}



/* GPIO Initialization Function */
 void MX_GPIO_Init(void) {
    GPIO_InitTypeDef GPIO_InitStruct = {0};

    /* Enable GPIO clock for PA9 and PA10 (USART1 TX/RX pins) */
      __HAL_RCC_GPIOA_CLK_ENABLE();

      /* Configure PA9 (USART1 TX) */
      GPIO_InitStruct.Pin = GPIO_PIN_9;
      GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;  // Alternate function push-pull
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
      GPIO_InitStruct.Alternate = GPIO_AF7_USART1;  // AF7 for USART1
      HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

      /* Configure PA10 (USART1 RX) */
      GPIO_InitStruct.Pin = GPIO_PIN_10;
      GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;  // Alternate function push-pull
      GPIO_InitStruct.Pull = GPIO_NOPULL;
      GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
      GPIO_InitStruct.Alternate = GPIO_AF7_USART1;  // AF7 for USART1
      HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}


 void USART1_UART_Init(void) {
   /* Enable USART1 clock */

 	 /* GPIO Ports Clock Enable */
 	    __HAL_RCC_GPIOC_CLK_ENABLE();
 	    __HAL_RCC_GPIOA_CLK_ENABLE();
 	    __HAL_RCC_GPIOB_CLK_ENABLE();
 	    __HAL_RCC_GPIOE_CLK_ENABLE();  // Enable clock for Port E
 	    __HAL_RCC_GPIOD_CLK_ENABLE();

   __HAL_RCC_USART1_CLK_ENABLE();

   /* Initialize USART1 */
   huart1.Instance = USART1;
   huart1.Init.BaudRate = 9600;
   huart1.Init.WordLength = UART_WORDLENGTH_8B;
   huart1.Init.StopBits = UART_STOPBITS_1;
   huart1.Init.Parity = UART_PARITY_NONE;
   huart1.Init.Mode = UART_MODE_TX_RX;
   huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
   huart1.Init.OverSampling = UART_OVERSAMPLING_16;

   if (HAL_UART_Init(&huart1) != HAL_OK) {
     Error_Handler();  // Handle initialization error
   }
 }


 /* System Clock Configuration */
 void SystemClock_Config(void) {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

     // Configure the main internal regulator output voltage
     if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) {
         Error_Handler();
     }

     // Initializes the RCC Oscillators according to the specified parameters
     // Here we use the internal Multi-Speed Internal (MSI) oscillator
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
     RCC_OscInitStruct.MSIState = RCC_MSI_ON;
     RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;  // MSI range 6 corresponds to 4 MHz
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
     RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
     RCC_OscInitStruct.PLL.PLLM = 1;
     RCC_OscInitStruct.PLL.PLLN = 40;
     RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
     RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
     RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
         Error_Handler();
     }

     // Initializes the CPU, AHB, and APB buses clocks
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
                                 | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) {
         Error_Handler();
     }

     // Enable MSI Auto-calibration
     HAL_RCCEx_EnableMSIPLLMode();
 }



/* Error Handler */
void Error_Handler(void) {
    __disable_irq();
    while (1) {
        // Blink the LED to indicate an error

        HAL_Delay(500);
    }
}

 

 

10 REPLIES 10
roystm321
Visitor

Ok i will try it, thanks