cancel
Showing results for 
Search instead for 
Did you mean: 

ULINK2 USB-JTAG of Keil and STM3210E-EVAL

levmalkin
Associate
Posted on November 09, 2008 at 07:55

ULINK2 USB-JTAG of Keil and STM3210E-EVAL

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
16-32micros
Associate III
Posted on May 17, 2011 at 12:51

Dear lev,

Welcome in our STM32 forums :)

Please take care that ''C:\Keil\ARM\Boards\Keil\MCBSTM32E\Blinky'' example and also the other ones under MCBSTM32E sub-directory are done on the following board from Keil and not from ST, so the hardware schematics are not the same.

I suggest you to download ST FW library :

http://www.st.com/stonline/products/support/micro/files/um0427.zip

, Next go to template project STM32F10xFWLib_v2.0.3\FWLib\project\RVMDK , then replace the files by the ones located in STM32F10xFWLib_v2.0.3\FWLib\examples\GPIO\IOToggle {You can have a look at readme.txt first} to know what is expected to RUN.

Hope this helps you. Enjoy it :)

Cheers,

STOne-32.

levmalkin
Associate
Posted on May 17, 2011 at 12:51

Shalom from JERUSALEM!

Here is my technical problem:

I've got STM3210E-EVAL evaluation board from ST company. -

target STM32F103ZE

I've tried to programm it's flash with ULINK2 USB-JTAG on the base of

simple led blinking test programm.

The flash programming is performing, but I cann't see results -

the programm not functions.

What can I do ?

Is it possible use ULINK2 USB-JTAG for STM3210E-EVAL board?

Some details:

OS : WINDOWS XP

IDE-Version:

µVision3 V3.63

Copyright (c) Keil Elektronik GmbH / Keil Software, Inc. 1995 - 2008

License Information:

LEV USER

COMPANY

LIC=----

Tool Version Numbers:

Toolchain: RealView MDK-ARM Version: 3.24

Toolchain Path: BIN31

C Compiler: Armcc.Exe V3.1.0.939 [Evaluation]

Assembler: Armasm.Exe V3.1.0.939 [Evaluation]

Linker/Locator: ArmLink.Exe V3.1.0.939 [Evaluation]

Librarian: ArmAr.Exe V3.1.0.939 [Evaluation]

Hex Converter: FromElf.Exe V3.1.0.939 [Evaluation]

CPU DLL: SARMCM3.DLL V3.24

Dialog DLL: DARMSTM.DLL V1.36

Target DLL: BIN\UL2CM3.DLL V1.43

Dialog DLL: TARMSTM.DLL V1.35

**************************************************

Listing of main:

int main (void) {

stm32_Init (); // STM32 setup

GPIO_WriteBit(GPIOF, GPIO_Pin_8, Bit_RESET);

GPIO_WriteBit(GPIOF, GPIO_Pin_8, Bit_SET); // Turn On Led

GPIO_WriteBit(GPIOF, GPIO_Pin_6, Bit_SET); // Turn On Led

while (1) {

}

}

**************************************************

Remark: ULINK2 USB-JTAG succesfully works with MCB2300 evaluation board of KEIL

Regards

Lev Malkin

:-[

jaroslaw2
Associate II
Posted on May 17, 2011 at 12:51

Hi,

1.Can you show us body of stm32_Init ();

2. Did you check pin boot0, should be connected to GND.