2010-10-20 2:49 AM
uClinux on STM3210E-Eval + STM32F103ZE
2011-05-17 5:11 AM
maybe it is relevant that i dont want(try) to use the NOR-flash version. i try to run the mcu-flash (internal flash) version.
some minutes ago i tried the first time the NOR-flash version and until now everything seems to be fine. so can i expect that there are two possible problems: 1. damaged internal flash 2. damaged sourcefiles or compiler or image ?? the least thing i could expect is that uclinux , against the guide, could not be run from internal flash memory. in the case, that it run perfectly from external flash, i think that something written in the guide is completly wrong refering to the problems i desribed above. am i right when i say that, its not possible to run uclinux in a stable way from internal flash? it would be nice if someone from st would say something to that. thanks2011-05-17 5:11 AM
nobody had an idea to this?
2011-05-17 5:11 AM
I tried getting it running on my clone board last weekend but failed :(
I could not even get it started... Will try again this weekend :)2011-05-17 5:11 AM
i solved the problem ''myself''.
after i tried running uclinux out of external flash and everything was fine i checked another board. and see - everything is fine. so question is answered at first. thanks2011-05-17 5:11 AM
So it was a hardware issue?
Last night I finally manage to recompile everything for my board. It starts, but due to my limited memory (512KB only) I immediately get a memory allocation failure when it tries to run linuxrc. Now to figure out how to tune this for better memory usage.