Posted on May 17, 2011 at 14:13success...i get it compiled now and i think all dependecies are right but when i run it on the board i get the following error: CPU: 0 Not tainted (2.6.26-uc0 #21) pc : [<680a9952>] lr : [<680a9f47>] psr: 610...
Posted on May 17, 2011 at 14:11i solved the problem ''myself''. after i tried running uclinux out of external flash and everything was fine i checked another board. and see - everything is fine. so question is answered at first. thanks
Posted on May 17, 2011 at 14:11maybe it is relevant that i dont want(try) to use the NOR-flash version. i try to run the mcu-flash (internal flash) version. some minutes ago i tried the first time the NOR-flash version and until now everything seems...