cancel
Showing results for 
Search instead for 
Did you mean: 

UART4 DMA Rx Problem

leventeyigel52
Associate II
Posted on April 04, 2014 at 13:21

I cannot get into DMA mode, the code  I wrote did not get into DMA  interrupt. The code I wrote is as follows. Any advice?( my processor is STM32F103ZG)

 uint8_t RxBuffer1[100]; 

 /*UART - Pin Config*/

  GPIO_InitTypeDef GPIO_InitStructure;

  USART_InitTypeDef USART_InitStructure;

  NVIC_InitTypeDef NVIC_InitStructure;

  DMA_InitTypeDef DMA_InitStructure;; 

  /* Clock configuration -------------------------------------------------------*/

  RCC_APB2PeriphClockCmd( UART_GPIO_CLK_TX | UART_GPIO_CLK_RX | RCC_APB2Periph_AFIO, ENABLE);

  RCC_APB1PeriphClockCmd(UART_CLK , ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2,ENABLE);

 

 /* Configure the GPIO ports( UART4 Transmit and Receive Lines) */ 

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Pin =  UART_TxPin;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(UART_GPIO_TX, &GPIO_InitStructure); 

 

/* Configure the UART4_Rx as input floating */

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

  GPIO_InitStructure.GPIO_Pin = UART_RxPin ;

  GPIO_Init(UART_GPIO_RX, &GPIO_InitStructure);

  

  USART_InitStructure.USART_BaudRate = 1200;

  USART_InitStructure.USART_WordLength = USART_WordLength_9b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_Even;

  USART_InitStructure.USART_HardwareFlowControl =     USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  

    /* UART Guard Time set to 16 Bit */

  USART_SetGuardTime(UART4, 8);

 

  USART_Init(UART4, &USART_InitStructure);

   /* Enable the UART4 */

  USART_Cmd(UART4, ENABLE);

  

  

  /************************* DMA *****************************/

  DMA_DeInit(DMA2_Channel3);

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&UART4->DR;

  DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)RxBuffer1; 

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; // Receive 

  DMA_InitStructure.DMA_BufferSize = 1; 

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; 

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; 

  DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; 

  DMA_InitStructure.DMA_Priority = DMA_Priority_High; 

  DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

 

  DMA_Init(DMA2_Channel3, &DMA_InitStructure); 

  /* Enable the USART Rx DMA request */

  USART_DMACmd(UART4, USART_DMAReq_Rx, ENABLE);

 

  /* Enable DMA Transfer Complete interrupt */

  DMA_ITConfig(DMA2_Channel3, DMA_IT_TC, ENABLE); 

 

  /* Enable the DMA RX Stream */

  DMA_Cmd(DMA2_Channel3, ENABLE);

  /* Enable the UART4 RX DMA Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = DMA2_Channel3_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);  

/*******************************************************************/ 

void DMA2_Channel3_IRQHandler()

{

  if(DMA_GetITStatus(DMA2_IT_TC3)){

    

    Uart_Interrupt_Handler();

    

    DMA_ClearITPendingBit(DMA2_IT_TC3);

  }

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
waclawek.jan
Super User
Posted on April 04, 2014 at 13:40

>

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; // Receive

?

JW

leventeyigel52
Associate II
Posted on April 04, 2014 at 13:47

Don't we choose ''DMA_DIR_PeripheralDST'' when interrupt comes Rx Pin ?

Posted on April 04, 2014 at 13:52

Don't we choose ''DMA_DIR_PeripheralDST'' when interrupt comes Rx Pin ?

NO, you're configuring a DMA transaction, which you want to READ the Peripheral register, and WRITE to Memory, this would mean the Peripheral is the SOURCE (SRC), right?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
leventeyigel52
Associate II
Posted on April 04, 2014 at 14:00

Is my BufferSize correct ? 

I want to get into IRQ for each byte ? 

leventeyigel52
Associate II
Posted on April 04, 2014 at 14:08

I changed the DMA_DIR_PeripheralDST to DMA_DIR_PeripheralSRC .

 

But i cannot still get into the interrupt 

Posted on April 04, 2014 at 14:37

If you use Normal mode you'll need to reinitialize the DMA on each interrupt

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
leventeyigel52
Associate II
Posted on April 04, 2014 at 14:54

I changed the DMA_InitStructure.DMA_Mode to  DMA_Mode_Circular but the problem has not solved. 

Is there an error on IRQ Configuring ?

leventeyigel52
Associate II
Posted on April 04, 2014 at 16:20

to be migrated, sourceId: 40316:697285D7-A9CA-445D-B16C-F23BF0E3B1A3

Posted on April 04, 2014 at 17:30

The last version is following below. I cannot understand where is the wrong ?

 

A cursory review suggests the code is not unreasonable, although I honestly can't see the point of doing a one byte DMA, and how that's materially more useful than just doing an RXNE interrupt.

Are you actually receiving any data? If you make a simple polled mode version, or echo back, does that actually work?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..