cancel
Showing results for 
Search instead for 
Did you mean: 

UART transmitter transmits wrong ascii value to my pc.

khairul_bashar
Associate

UART transmitter transmits wrong ascii value to my pc.

what is the problem in my code..??

I put a charecter in Data Register, but serial terminal show another ascii code.

My IDE is KeiluVision5. the code is in below.....

 

 

#include<stdint.h>
#include<stdio.h>
#include<stm32f446xx.h>
 
#define GPIOAEN (1U<<0)
#define UART2EN (1U<<17)
 
#define CR1_TE (1U<<3)
#define CR1_UE (1U<<13)
#define SR_TXE (1U<<7)
 
#define SYS_FREQ 45000000
#define APB1_CLK SYS_FREQ
 
#define UART_BAUDRATE 115200
 
void uart2_tx_init(void);
void uart2_write(uint8_t ch);
static void uart_set_baudrate(USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t BaudRate);
static uint16_t compute_uart_bd(uint32_t PeriphClk, uint32_t BaudRate);
 
 
 
 
int main(void){
 
uart2_tx_init();
 
while(1){
 
uart2_write('z');
for(int i=0;i<1000000;i++){}
}
 
}
 
 
 
 
 
void uart2_write(uint8_t ch){
 
//********************************************************
// make sure tranmit data register is empty
while(!(USART2->SR & SR_TXE)){}
 
//write to the transmit data register
USART2->DR = (ch & 0xFF);
 
 
}
 
 
void uart2_tx_init(void){
 
//***************configure GPIO PIN****************
//enabling clock access on GPIOA
RCC->AHB1ENR |= GPIOAEN;
 
//set PA2 as Alternate function mode
GPIOA->MODER &= ~(1U<<4);
GPIOA->MODER |= (1U<<5);
 
// set alternate function type AF07
GPIOA->AFR[0] |= (1U<<8);
GPIOA->AFR[0] |= (1U<<9);
GPIOA->AFR[0] |= (1U<<10);
GPIOA->AFR[0] &= ~(1U<<11);
 
 
//***************configure UART****************
//enable clock access to usart2
RCC->APB1ENR |= UART2EN;
 
//configure baudrate
uart_set_baudrate(USART2, APB1_CLK, UART_BAUDRATE);
 
//configure data transfer direction
USART2->CR1 |=CR1_TE;
 
//Enable uart module
USART2->CR1 |=CR1_UE;
 
}
 
 
 
static void uart_set_baudrate(USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t BaudRate){
 
USARTx->BRR = compute_uart_bd(PeriphClk, BaudRate);
 
}
 
 
 
static uint16_t compute_uart_bd(uint32_t PeriphClk, uint32_t BaudRate){
 
//uint16_t abc = ((PeriphClk + (BaudRate/2))/ BaudRate);
 
//printf("abc");
 
return (uint16_t)((PeriphClk + (BaudRate/2))/ BaudRate);
 
 
}
 
 
 
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Super User

The most common reasons are a baudrate mismatch between transmitter and receiver or some different code page/char translation done by "intelligent" terminal progs on the receiver side. Check the signals on the wire using a scope or a cheap logic analyzer.

hth

KnarfB

View solution in original post

2 REPLIES 2
KnarfB
Super User

The most common reasons are a baudrate mismatch between transmitter and receiver or some different code page/char translation done by "intelligent" terminal progs on the receiver side. Check the signals on the wire using a scope or a cheap logic analyzer.

hth

KnarfB

khairul_bashar
Associate

Thank you for your suggestion.