UART STM32F429 & STM32F407 discovery
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-13 12:05 AM
Posted on June 13, 2014 at 09:05
Hi,
I'm testing the two discovery STM32F429 and STM32F407. What I've done so far is that the 429 sends data to the 407 through UART4. The 407 interrupts at every character received, and all works fine! If I do the opposite (the 407 sends data to the 429) nothing happens. I'm using the same code and I don't understand why it works only in a verse. I tried to use a different RX pin on the 429, but nothing changes. The only thing different is that I'm using the USB (not OTG) with the 429 to print to PC the characters (not) received from the 407. Thanks, Pierpaolo
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0