cancel
Showing results for 
Search instead for 
Did you mean: 

TXE interrupt comes even though TXEIE is not enabled

rodi66
Visitor

Basic setting of USART2: DMA Transfer and receive via interrupt as RS485.

As long as only DMA transfer is ongoing, all will be ok. At first time a receive interrupt will occur, the transmit will trigger an interrupt, even though no TXEIE is set. This crashes the system 

The same settings for UART5 and USART3: there it works fine without problems (RS232 or RS485).

Whats going wrong, or some errata for this behavior?

MCU type: STM32F756

0 REPLIES 0