cancel
Showing results for 
Search instead for 
Did you mean: 

Two USARTs

nygaard
Associate II
Posted on February 07, 2014 at 15:23

Hi,

I am trying to use two USARTs at the same time, but I can't get it to work.

First:

void RCC_Configuration(void)

{

  /* USART1 clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

  /* USART2 clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

  /* GPIOA clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

}

Then:

void GPIO_Configuration(void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  /* GPIO Configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  /* Connect USART pins to AF */

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7);   // USART1_TX

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7);  // USART1_RX

  /* GPIO Configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  /* Connect USART pins to AF */

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7);   // USART2_TX

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7);  // USART2_RX

}

And finally:

void USART1_Configuration(void)

{

  USART_InitTypeDef USART_InitStructure;

  /* USARTx configuration ------------------------------------------------------*/

  /* USARTx configured as follow:

        - BaudRate = 115200 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART_InitStructure.USART_BaudRate = 115200; //115200;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART1, &USART_InitStructure);

  USART_Cmd(USART1, ENABLE);

}

void USART2_Configuration(void)

{

  USART_InitTypeDef USART_InitStructure;

  /* USARTx configuration ------------------------------------------------------*/

  /* USARTx configured as follow:

        - BaudRate = 115200 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART_InitStructure.USART_BaudRate = 115200; //115200;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART2, &USART_InitStructure);

  USART_Cmd(USART2, ENABLE);

}

And of cause i am calling them all from main:

  RCC_Configuration();

  GPIO_Configuration();

  USART1_Configuration();

  USART2_Configuration();

But I can only send data via USART 1... What can be wrong?!

Kind regards,

Michael

#usart #discovery #stm32
2 REPLIES 2
Posted on February 07, 2014 at 15:26

 /* USART2 clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

APB1 !! APB1 !!
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nygaard
Associate II
Posted on February 10, 2014 at 09:12

Friday + copy+paste + DO'H (http://www.youtube.com/watch?v=g6GuEswXOXo)! 

But thanks! :-)

Kind regards,

Michael