cancel
Showing results for 
Search instead for 
Did you mean: 

TWO STM32F4 Discovery Boards Communication Using SPI1

adarsh
Associate II
Posted on March 18, 2015 at 11:50

The original post was too long to process during our migration. Please click on the attachment to read the original post.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on March 24, 2015 at 11:19

Here some recommendations:

1- Use the ''Format Code Block'' feature when editing your message. This helps to read & review easily your code.

2- Review the pins assignment in your code compared to the datasheet of used product.

3- Try to start from a working example like the ones available in the STM32F4 standard peripheral package (STM32F4xx_DSP_StdPeriph_Lib_V1.5.0\Project\STM32F4xx_StdPeriph_Examples\SPI).

You may update it according to your needs. You find there a readme file describing how to test the examples.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AvaTar
Lead
Posted on March 24, 2015 at 11:50

Please check with the code and give me solution.

 

Thanks in advance and please reply me back soon, I'm in deadline of my work.

 

From the other one's perspective, do you really consider this helpful ?