cancel
Showing results for 
Search instead for 
Did you mean: 

Two NUCLEO-H755ZI-Q boards acting differently

SoCalJim
Associate III

I have two NUCLEO-H755ZI-Q boards and I’m trying to run the SPI_FullDuplex_ComIT example on both.

One board breaks here (whether the software is built for master or slave):

snap03740.jpg

The other board has no problem (whether the software is built for master or slave).

Any ideas?

1 ACCEPTED SOLUTION

Accepted Solutions

@SoCalJim wrote:

Should CM4 be enabled? Should CM7 be enabled as well? Both are enabled on the working board.


Your log shows that CM4 is disabled. Both CM7 and CM4 should be enabled.

Of course CM4 needs to be activated as there is a synchronization mechanism implemented in the example:

 

  /* Wait until CPU2 boots and enters in stop mode or timeout*/
  timeout = 0xFFFF;
  while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
  if ( timeout < 0 )
  {
    Error_Handler();
  }

 

If CM4 is disabled you will be infinitely looped in this while loop as CM7 is waiting for a signal from CM4 that never generated.

So please confim that by enabling CM4 (as I showed previously) the issue is solved. Or comment out that while loop.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

14 REPLIES 14
SofLit
ST Employee

Hello,

Check if you have disabled CM4 in the option byte.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

BCM4 was set. I cleared it using:

./STM32_Programmer_CLI -c port=SWD -ob BCM4=0x0

I verified it’s clear. Unfortunately, the problem persists.

 

I looked at the working board and found both BCM4 and BCM7 are set, just like non-working board. The command

STM32_Programmer_CLI -c port=SWD -ob displ

showed no differences between the boards.

Try to use STM32CubeProgrammer and check if the CM4 is enabled in the option byte.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.18.0
      -------------------------------------------------------------------

ST-LINK SN  : 0048001B3433510A37363934
ST-LINK FW  : V3J15M7
Board       : NUCLEO-H755ZI-Q
Voltage     : 3.29V
SWD freq    : 8000 KHz
Connect mode: Normal
Reset mode  : Software reset
Device ID   : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size  : 2 MBytes
Device type : MCU
Device CPU  : Cortex-M7/M4
BL Version  : 0x91


UPLOADING OPTION BYTES DATA ...

  Bank          : 0x00
  Address       : 0x5200201c
  Size          : 308 Bytes

██████████████████████████████████████████████████ 100%


OPTION BYTES BANK: 0

   Read Out Protection:

     RDP          : 0xAA (Level 0, no protection)

   BOR Level:

     BOR_LEV      : 0x0 (reset level is set to VBOR0)

   User Configuration:

     IWDG1_SW     : 0x1 (Independent watchdog is controlled by software)
     IWDG2_SW     : 0x1 (Independent watchdog is controlled by software)
     NRST_STOP_D1 : 0x1 (STOP mode on Domain 1 is entering without reset)
     NRST_STBY_D1 : 0x1 (STANDBY mode on Domain 1 is entering without reset)
     FZ_IWDG_STOP : 0x1 (Independent watchdog is running in STOP mode)
     FZ_IWDG_SDBY : 0x1 (Independent watchdog is running in STANDBY mode)
     SECURITY     : 0x0 (Security feature disabled)
     BCM4         : 0x0 (CM4 boot disabled)
     BCM7         : 0x1 (CM7 boot enabled)
     NRST_STOP_D2 : 0x1 (STOP mode on Domain 2 is entering without reset)
     NRST_STBY_D2 : 0x1 (STANDBY mode on Domain 2 is entering without reset)
     SWAP_BANK    : 0x0 (after boot loading, no swap for user sectors)
     IO_HSLV      : 0x0 (Product working in the full voltage range, I/O speed optimization at low-voltage disabled)

   Boot address Option Bytes:

     BOOT_CM7_ADD0: 0x800  (0x8000000)
     BOOT_CM7_ADD1: 0x1FF0  (0x1FF00000)
     BOOT_CM4_ADD0: 0x810  (0x8100000)
     BOOT_CM4_ADD1: 0x1000  (0x10000000)

   PCROP Protection:

     PROT_AREA_START1: 0xFF  (0x800FF00)
     PROT_AREA_END1: 0x0  (0x80000FF)
     DMEP1        : 0x0 (Flash Bank 1 PCROP zone is kept when RDP level regression (change from level 1 to 0) occurs)
     PROT_AREA_START2: 0xFF  (0x810FF00)
     PROT_AREA_END2: 0x0  (0x81000FF)
     DMEP2        : 0x0 (Flash Bank 2 PCROP zone is kept when RDP level regression (change from level 1 to 0) occurs)

   Secure Protection:

     SEC_AREA_START1: 0xFF  (0x800FF00)
     SEC_AREA_END1: 0x0  (0x80000FF)
     DMES1        : 0x0 (Flash Bank 1 secure area is kept when RDP level regression (change from level 1 to 0) occurs)
     SEC_AREA_START2: 0xFF  (0x810FF00)
     SEC_AREA_END2: 0x0  (0x81000FF)
     DMES2        : 0x0 (Flash Bank 2 secure area is kept when RDP level regression (change from level 1 to 0) occurs)

   DTCM RAM Protection:

     ST_RAM_SIZE  : 0x0 (2 KB)

   Write Protection:

     nWRP0        : 0x1 (Write protection not active on this sector)
     nWRP1        : 0x1 (Write protection not active on this sector)
     nWRP2        : 0x1 (Write protection not active on this sector)
     nWRP3        : 0x1 (Write protection not active on this sector)
     nWRP4        : 0x1 (Write protection not active on this sector)
     nWRP5        : 0x1 (Write protection not active on this sector)
     nWRP6        : 0x1 (Write protection not active on this sector)
     nWRP7        : 0x1 (Write protection not active on this sector)
     nWRP8        : 0x1 (Write protection not active on this sector)
     nWRP9        : 0x1 (Write protection not active on this sector)
     nWRP10       : 0x1 (Write protection not active on this sector)
     nWRP11       : 0x1 (Write protection not active on this sector)
     nWRP12       : 0x1 (Write protection not active on this sector)
     nWRP13       : 0x1 (Write protection not active on this sector)
     nWRP14       : 0x1 (Write protection not active on this sector)
     nWRP15       : 0x1 (Write protection not active on this sector)
BCM4         : 0x0 (CM4 boot disabled)

The log shows that CM4 is disabled.

Please use STM32CubeProgrammer in graphical mode to enable it:

SofLit_0-1738269264025.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

The project is SPI_FullDuplex_ComIT_CM7:

 

snap03743.jpg

Should CM4 be enabled? Should CM7 be enabled as well? Both are enabled on the working board.


@SoCalJim wrote:

Should CM4 be enabled? Should CM7 be enabled as well? Both are enabled on the working board.


Your log shows that CM4 is disabled. Both CM7 and CM4 should be enabled.

Of course CM4 needs to be activated as there is a synchronization mechanism implemented in the example:

 

  /* Wait until CPU2 boots and enters in stop mode or timeout*/
  timeout = 0xFFFF;
  while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
  if ( timeout < 0 )
  {
    Error_Handler();
  }

 

If CM4 is disabled you will be infinitely looped in this while loop as CM7 is waiting for a signal from CM4 that never generated.

So please confim that by enabling CM4 (as I showed previously) the issue is solved. Or comment out that while loop.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

snap03745.jpg

snap03744.jpg