2014-07-24 1:18 PM
Does anyone have any experience running two applications on single processor?
I have accomplished running two separate images that can communicate with each other with function pointer (callbacks) on other processors by using dlls, but I can’t find information about doing so on a Cortex processor.
This should allow the applications to be built separately.2014-07-30 1:10 PM
Well it would depend a lot if the task actually needs a 6.25 HP Briggs and Stratton, or 1200 HP Bugatti Veyron engine.
2014-07-31 10:13 AM
I don't really need the horsepower of a dual core. In the past my product was done on two processors, one 32-bit and one 8-bit. Now the physical size and cost are driving me to look into other options. The issue is that:
1) I don't control the code in the 8-bit processor 2) The two applications need to be independently programmable. I don't have the time to do a 'proof of concept' at the moment so I was hoping someone could point me to an example, app note ...2014-07-31 10:40 AM
2014-07-31 11:07 AM
You may find NXP's LPC 4300 microcontrollers interesting. These have a Cortex-M4 CPU and a Cortex-M0 CPU. I don't know if your separate programability goals can be entirely achieved with this device though.