Trying to make use of the stm32f10x_stdperiph library in Keil IDE
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2010-05-28 9:01 AM
Posted on May 28, 2010 at 18:01
Trying to make use of the stm32f10x_stdperiph library in Keil IDE
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:52 AM
Posted on May 17, 2011 at 13:52
I'm familiar with the V2 library, and Keil uv3
Pretty sure you build the libraries in-place (using their own Project), and then bring the compiled library in, not the individual source files. Your project should reference the include files for the library, and the library (..\??\..\RV31\LIB\ST\STM32F10xR.LIB, or whatever) itself
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:52 AM
Posted on May 17, 2011 at 13:52
''you build the libraries in-place (using their own Project), and then bring the compiled library in, not the individual source files.''
You can do it either way -whichever you prefer.''* How to set-up the include-path (i know where to apply the paths but jsut not which ones to add)'' The ones which contain the necessary files! Your error says that ''uint32_t'' is undefined - so you're obviously missing a file which defines that!''* which files to copy in the project in Keil''
You don't have to copy any files - you can copy them if you wish, or you can just add them to the Project in their original location.''* Does the Keil environment need to have some of the files located in some specific folders?'' No - you just need to ensure that your project is configured to find them wherever they are located.
From: clive1
Posted: Saturday, May 29, 2010 3:56 AMSubject: Trying to make use of the stm32f10x_stdperiph library in Keil IDEI'm familiar with the V2 library, and Keil uv3
Pretty sure you build the libraries in-place (using their own Project), and then bring the compiled library in, not the individual source files. Your project should reference the include files for the library, and the library (..\??\..\RV31\LIB\ST\STM32F10xR.LIB, or whatever) itself
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
A complex system designed from scratch never works and cannot be patched up to make it work.