2024-08-27 01:39 PM
I'm studying and discovering how to create custom bootloader for STM32F7 MCU.
I starting with looking at official ST docs, eg. AN4854 "In-application programming with SD cards and examples" docs (AN4854 pdf, readme.txt from en.x-cube-iap-sd sources files archive) and available source files, and I have found that
for STM32L476G-EVAL board program (as I understand it is bootloader) "size is 13 Kbytes" and user application starting from address 0x0800E000 (that is 56Kbytes offset from 0x08000000). Compiling source files, I got STM32L476G_EVAL.bin file with size 44.712 bytes (or almost 44 Kbytes).
I can't figure out why docs state that "program is about 13 Kbytes" while bin size is 44 Kbytes and why there used such larger than bootloader offset E000 (56Kbytes instead stated 13 KBytes). Than what is "The image is uploaded with the IAP from the STM32L4xx, size 4 Kbytes".
Same question for STM32072B-EVAL implementation about stated sizes and offsets.
Thank you for any explanation how to understand all these or may be there mistakes?
P.S. original readme.txt (documentation) from en.x-cube-iap-sd.zip is attached
2024-08-27 04:21 PM
Several things going on here.
a) The granularity of the Flash blocks, whether they are small, uniform in size, different sized, or large
You have a lot less flexibility when the Flash blocks when they are 128 KB in size than you do with 2 or 4 KB
The trade here is the size your loader can take, or what the maximum size is before you end up wasting a lot of blank space.
b) If the Cortex-M can relocate the Vector Table to an address deeper into Flash. The original CM0 doesn't provide SCB->VTOR, so to get a secondary app, you need to remap the RAM to Zero, and copy in a new vector table into the root.
The F77x has 16KB, 64KB and 128KB blocks, and double those with side-to-side banking.