2019-11-17 3:28 AM
No source file named C:\\vmi\\viber_x4\\x4_fw_1_1\\BootLoader\\SRC\\bl_main.c.
Program received signal SIGTRAP, Trace/breakpoint trap.
GR_IconMenu (iconSTR=0x23a0008, Options=0) at ..\..\COMMON\SRC\GraphMenus.c:151
151 if (xCount == 0)
Halted to watchpoint
Core context saved
Load the program in memory
Loading section .fastcode, size 0x7050 lma 0x0
Loading section .isr_vector, size 0x298 lma 0x20000000
Loading section .fastdata, size 0xc0 lma 0x20000298
Loading section .text, size 0x49f90 lma 0x70000000
Loading section .ARM, size 0x8 lma 0x70049f90
Loading section .rodata, size 0x9668 lma 0x71200000
Loading section .init_array, size 0x4 lma 0x71209668
Loading section .fini_array, size 0x4 lma 0x7120966c
Loading section .data, size 0x196c lma 0x71209670
Start address 0x70000eb0, load size 377628
Transfer rate: 96 KB/sec, 2839 bytes/write.
Program loaded
CPU context restored
Abort any bootloader task
Temporary breakpoint 4 at 0x70027f3a: file ..\SRC\VX4_Main.c, line 126.
Launch the program using the bootloader
$1 = 1520805210
warning: Remote failure reply: E31
/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Quit this debugging session? (y or n) [answered Y; input not from terminal]
C:\Users\fb\AppData\Local\Temp\truestudio6664351465486505174gdbscript:64: Error in sourced command file:
Remote communication error. Target disconnected.: No error.
This is a bug, please report it. For instructions, see:
<http://www.gnu.org/software/gdb/bugs/>.
/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Create a core file of GDB? (y or n) [answered Y; input not from terminal]