cancel
Showing results for 
Search instead for 
Did you mean: 

trouble with stm32f4 and 16x2 lcd after moving from C to C++

Bogdan
Senior
Posted on June 17, 2014 at 00:59

Hi

after moving a whole project from C to a c++ project, had trouble with the lcd librarry.

On the C project, the library works fine. But in C++ i get the following error

Error[Pe513]: a value of type ''int'' cannot be assigned to an entity of type ''TLCD_NAME_t'' 

Error[Pe511]: this operation on an enumerated type requires an applicable user-defined operator function

This is the initial declaration of TLCD_NAME

typedef enum

{

  TLCD_RS = 0,  // RS-Pin

  TLCD_E  = 1,  // E-Pin

  TLCD_D4 = 2,  // DB4-Pin

  TLCD_D5 = 3,  // DB5-Pin

  TLCD_D6 = 4,  // DB6-Pin

  TLCD_D7 = 5   // DB7-Pin

}TLCD_NAME_t;

This is the code

where it points the error

 

GPIO_InitTypeDef  GPIO_InitStructure;

  TLCD_NAME_t lcd_pin;

  

for(lcd_pin=0;lcd_pin<TLCD_ANZ;lcd_pin++) {

    // Clock Enable

    RCC_AHB1PeriphClockCmd(LCD_2X16[lcd_pin].TLCD_CLK, ENABLE);

GPIO_InitStructure.GPIO_Pin = LCD_2X16[lcd_pin].TLCD_PIN;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  

Ok, from what i mannaged to understand is that it wont let me assign numbers to its structure positions, why? How can i increment each position of it?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0