2014-06-16 03:59 PM
Hi
after moving a whole project from C to a c++ project, had trouble with the lcd librarry. On the C project, the library works fine. But in C++ i get the following error Error[Pe513]: a value of type ''int'' cannot be assigned to an entity of type ''TLCD_NAME_t'' Error[Pe511]: this operation on an enumerated type requires an applicable user-defined operator function This is the initial declaration of TLCD_NAMEtypedef enum
{ TLCD_RS = 0, // RS-Pin TLCD_E = 1, // E-Pin TLCD_D4 = 2, // DB4-Pin TLCD_D5 = 3, // DB5-Pin TLCD_D6 = 4, // DB6-Pin TLCD_D7 = 5 // DB7-Pin }TLCD_NAME_t;This is the code
where it points the errorGPIO_InitTypeDef GPIO_InitStructure;
TLCD_NAME_t lcd_pin;for(lcd_pin=0;lcd_pin<TLCD_ANZ;lcd_pin++) {
// Clock Enable RCC_AHB1PeriphClockCmd(LCD_2X16[lcd_pin].TLCD_CLK, ENABLE); GPIO_InitStructure.GPIO_Pin = LCD_2X16[lcd_pin].TLCD_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; Ok, from what i mannaged to understand is that it wont let me assign numbers to its structure positions, why? How can i increment each position of it?