cancel
Showing results for 
Search instead for 
Did you mean: 

trouble with stm32f334r8 ADC which goes in to the unknown state in very weak noisy environment.

jkama
Associate

I am using stm32f334 in a power conversion project.

I have configured its ADC in  independent mode and transfer its data by two channel DMA.

some times in a even very weak noisy environment the ADC goes into the unknown state. I checked all of its register in that state but every thing was ok. Its DMA was working correctly in that state. I checked the statues of leg register but that register had not changed. it seems that source of analog input of ADC has changed.

I think that with regarding to above condition the stm32f334r8 in not suitable for power conversion at all.

do you know how I can resolve that problem?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0