Trouble with EXTI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 1:24 PM
Hi, I am having some troubles getting EXTI0 working properly with GPIOA.P0. At present, the interrupt works, just in the wrong way. I have a push button hooked up to GPIOA.P0 that pulls it to ground. It is configured as input/pull-down. However, I put a breakpoint in the interrupt routine, and it's called if the button is not pressed. So if I start the program while holding the button down, it runs, and as soon as I let up on the button, it triggers the interrupt. I would like the interrupt to behave in the opposite manner, that it will trigger when the button is pressed. I have tried changing between rising/falling edge, but it does the same thing. Any suggestions? Thanks.
Here is my code:#include ''stm32f10x.h''#include ''stm32f10x_exti.h''
void EXTI0_IRQHandler(void)
{
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
// ...
int i =0;
i++;
/* Clear the EXTI line pending bit */
EXTI_ClearITPendingBit(EXTI_Line0);
}
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC->APB2ENR |= 0x51FD;
//RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC , ENABLE);
//configure as pull-down
GPIOC->CRL = 0x08;
GPIOC->ODR = 0x0000;
}
void EXTI_Configuration(void)
{
RCC->APB2ENR |= RCC_APB2ENR_AFIOEN; // enable clock for Alternate Function
GPIO_EXTILineConfig(GPIO_PortSourceGPIOA, GPIO_PinSource0);
EXTI_ClearITPendingBit(EXTI_Line0);
EXTI->IMR |= 0x01; // unmask interrupt
EXTI->EMR |= 0x01 ; // unmask event
EXTI->RTSR &= ~0x01 ; // set rising edge
EXTI->FTSR |= 0x01 ; // set falling edge
NVIC->ISER[0] |= (1 << (EXTI0_IRQn & 0x1F)); // enable interrupt EXTI 0
}
int main()
{
GPIO_Configuration();
EXTI_Configuration();
while(1)
{
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 2:06 PM
I have a push button hooked up to GPIOA.P0 that pulls it to ground. It is configured as input/pull-down.
Can you diagram that, and how it gets to be high? The library example looks likevoid EXTI0_Config(void)
{
/* Enable GPIOA clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
/* Configure PA.00 pin as input floating */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable AFIO clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);
/* Connect EXTI0 Line to PA.00 pin */
GPIO_EXTILineConfig(GPIO_PortSourceGPIOA, GPIO_PinSource0);
/* Configure EXTI0 line */
EXTI_InitStructure.EXTI_Line = EXTI_Line0;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; // or Falling if button shorts to ground
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable and set EXTI0 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
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
‎2013-03-22 2:16 PM
Thanks for the reply! Here are some pictures of my simple setup:
http://imgur.com/a/iq35gThe white goes to PC.0, and the striped red/brown wire to ground.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 2:22 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 2:25 PM
Again how does this get to be high?
Don't you need a 10K or 47K or something to the 3V rail on the white wire side of the switch (PC0). That or configure the input with an internal pull up?Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 4:13 PM
Honestly, I'm not sure. That's just how I've been doing pull-down with buttons. Do I need a resistor? And one more question, I can't see in the reference manual where it talks about NVIC priority. So if I want another interrupt, how do I set it to be a higher priority, just make those two values higher? Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-22 4:43 PM
http://elinux.org/File:EGHS-PullUpDownSwitch.jpg
You could have all interrupts at the same priority, it wouldn't really make much difference unless you want certain ones to preempt (interrupt) others. The NVIC is part of the ARM Cortex-M3 core, you could review some manuals from ARM's site, or Joseph Yiu's books on the core. ST also has a Programming Manual (not the flash one) which describes the M3/M4 cores.http://www.st.com/web/en/resource/technical/document/programming_manual/CD00228163.pdf
Up vote any posts that you find helpful, it shows what's working..