2025-06-02 8:08 AM
Hello,
I was wondering about the reasons to supply external clocks to the N6 MCU, since it seems that via HSI and LSI there are clocks integrated into the MCU.
I am having trouble to understand whether the internal clocks can satisfy my requirements:
- I don't have special accuracy requirements for LSE/LSI nor HSI/HSE
- I am using the CSI-2 interface
- I am using SPI and UART Interface
Are there reasons to supply external clocks?
Are there other considerations that I might have to take into account? (especially for example considering data rates of the interfaces that I am using or other)
Best Regards
Lucas
Solved! Go to Solution.
2025-06-02 9:41 AM
Generally it's things like Ethernet, USB and CAN which have critical timing expectations / standards.
Async UART does not, and can tolerate several percent error. Synchronous, where you provide the clocking, like SPI or camera sources, providing a clock, also generally safe.
2025-06-02 9:41 AM
Generally it's things like Ethernet, USB and CAN which have critical timing expectations / standards.
Async UART does not, and can tolerate several percent error. Synchronous, where you provide the clocking, like SPI or camera sources, providing a clock, also generally safe.